(0)| 5/2/2025 3:20 PM | |
|
Joined: 3/6/2020 Last visit: 7/3/2025 Posts: 40 Rating:
|
I use PG M4 and I installed new version of Win10 (there was no other software, just bare Windows and all updates) I have Edition Windows 10 Pro There is log [attached]
Attachment0502_Log.txt (154 Downloads) |
Last edited by: Moderator_Lan at: 05/02/2025 16:21:40Image embedded / Log attached |
|
| 5/2/2025 7:40 PM | |
|
Joined: 7/11/2024 Last visit: 12/30/2025 Posts: 200 Rating:
|
Helo plcspace I would check the following: - Run the installation with admin rights - Disable any firewall/ antivirus installed on the computer while the software is installed - Make sure that your system meets all the installation requirements described in the section "Important installation files" of the download page: SIMATIC STEP 7 incl. Safety, S7-PLCSIM and WinCC V20 TRIAL Download If none of this works, you should provide Siemens the full log so they can help you: Create a Support Request Good luck!! |
|
If this post has been useful, don't forget to rate it!😊 |
|
Follow us on