5/6/2025 11:16 AM | |
Joined: 4/29/2025 Last visit: 5/6/2025 Posts: 1 Rating:
|
Hi guys, I am working on s71200 plc, which is installed on site. the Scada is Tia portal v20 Professional. since the existing system is providing monitoring only, no control, so i made some amendments in the plc program and also created new tags for input and output. Now when i work on the SCADA pc, add buttons for ON/OFF but cannot connect with the plc. And create some internal tags and start simulation but cannot connect ,internal tags also not communicate . any advice on this will be appreciated. Thanks in advance ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 05/06/2025 11:54:37New subject after splitting |
|
Follow us on