5/7/2025 10:46 AM | |
Joined: 8/11/2023 Last visit: 8/27/2025 Posts: 5 Rating:
|
Hi, I am using 314-2PN/DP and CP-341 Modbus Master and trying to communicate with the Janitza energy analyzer. The CPU has no error. Only TX LED is blinking on CP-341, and the slave device not responding. I checked the wiring through ADAM Modbus device and slave device responding fine. I read the multiple manuals but not able to communicate. Sometime, I am getting error of 830 on P_SEND_RK block. Any help would be appreciated. THANKS.
------------------------------------------------------------------------------------------ Attachments7-300 MODBUS.zip (79 Downloads) |
Last edited by: abdullah.munawar at: 05/07/2025 10:51:24Last edited by: Moderator_Lan at: 05/07/2025 10:54:14New subject after splitting Last edited by: abdullah.munawar at: 05/08/2025 09:12:26. |
|
Follow us on