5/12/2025 8:07 PM | |
Joined: 12/18/2014 Last visit: 9/8/2025 Posts: 35934 Rating:
|
What do you mean with pre-program? And what is a small project for you?
What flow? You don't write anything about where flow data come.
Start a pump? Have you more pumps? In your first topic you ask your changing pumps: Help needed: Alternating two pumps in Siemens LOGO! Soft Comfort
Helping? Yes. Write a complete program? No. Then ask for step by step. |
5/12/2025 10:06 PM | |
Joined: 4/11/2022 Last visit: 8/26/2025 Posts: 90 Rating:
|
Hi mate, Your description is a little bit strange when you say...
I supposed that fault alarm should be launch when reach a threshold, right??? If you need the inverse, now it is easy to edit as you want. Anyway, find attahced my idea with alarm when reach threshold, example with number 150 in (B005). I used the LOGO 8.4 and flow signal thru Analog input AI1. Hope it open up your mind! AttachmentExample.zip (197 Downloads) |
Rgds, |
|
This contribution was helpful to
2 thankful Users |
Follow us on