6/2/2025 1:19 PM | |
Joined: 8/3/2009 Last visit: 9/3/2025 Posts: 16322 Rating:
|
Hello do you mean this example: https://support.industry.siemens.com/cs/de/en/view/109477071 Yes we used this on a WinCC Advanced RT station in the past. the application example is a bit complicated to get through and also if you want to expand or change anything you have to get deep into the code. If you have troube with the scripts use an internal tag to count up in the code or use the systemfunction "ShowSystemAlarm" for troubleshooting. The Link is just an example if you wan to adapt it you have to understand whats going on in the code/project. Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on