6/24/2025 11:52 AM | |
Joined: 3/30/2020 Last visit: 9/12/2025 Posts: 5446 Rating:
|
[Link: Library for Data Streams (LStream)] Study of the documentation provided with the public library may be helpful. |
Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
This contribution was helpful to
1 thankful Users |
6/26/2025 6:18 AM | |
Joined: 6/1/2006 Last visit: 9/9/2025 Posts: 144 Rating:
|
Hello Ashok, |
This contribution was helpful to
2 thankful Users |
6/26/2025 8:20 PM | |
Joined: 9/15/2006 Last visit: 9/10/2025 Posts: 543 Rating:
|
Massive warning using this library. The Deserialize function is full of basic programming beginners bugs, like wrong array offsets. Then overwriting the last element in the tree, not using the context of one element when searching for a value, and so on and so on. I wasted several hours fixing the errors, then I gave up and written my own parser, which also took magnitudes less memory if you have to parse a big json file but only need some specific values. The http library has bugs as well, seems Siemens cannot read the RFCs. Seems all these libraries are written by students. |
Last edited by: Thomas_v2.1 at: 06/26/2025 20:21:30 |
|
This contribution was helpful to
1 thankful Users |
Follow us on