4/4/2023 4:06 AM | |
Posts: 2 Rating:
|
Hello, I need to receive data from a Mitsubishi PLC, I found an instruction from Siemens on how to receive data from there using the LCCF library and the "LCCF_MCClient" block using the Melsec protocol, tell me any information about this library, I did not find anything on the Internet AttachmentinfoPLC_net_109813439_MC_Client_V1.0_en.pdf (571 Downloads) |
7/2/2025 8:25 AM | |
Joined: 3/30/2020 Last visit: 9/12/2025 Posts: 5446 Rating:
|
[Link:MC Client – exchanging process data with Mitsubishi control systems]
The person you try to reach may not be available anymore. Maybe some of my thoughts helps, eve if I have not worked with the library. Page 21 of the manual provided on the support page, mentions a procedure that must be followed to write a value to a tag. I am guessing that it is important that these steps be followed very strictly. Please refer to the manual and see if there is some detail missed. I assume the Mitsubishi does not have write protect / security features on their PLC. Other than that - At the bottom of the support page is the ability to create a note / support request. Use this space in the attempt to reach the designer of the library. Mention with hardware and software is used om both Siemens and Mitsubishi side. |
Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
This contribution was helpful to
1 thankful Users |
Follow us on