7/14/2025 1:42 PM | |
Joined: 8/3/2009 Last visit: 9/15/2025 Posts: 16409 Rating:
|
Hello xoptopus WinCC V8.1 should be compatible with MS Server 2022 (like listed in compatibility list) does the Webconfigurator runs without problems? Check after the run and a PC restart if the IIS Website with Webnavigator is running in IIS Bye Murof |
If this Information really helps, you could use the Rate function |
|
7/16/2025 4:46 AM | |
Joined: 7/11/2025 Last visit: 7/17/2025 Posts: 2 Rating:
|
Hi Murof, I seem to have resolved the IIS issues. However, now the webnavigator won't connect. I'm getting the "failed to load https://XXX.XXX.XXX.XXX:4430/mainmenu.pd_" error. I don't understand. I'm doing everything according to Siemens' own documentation, but the system isn't working on Server 2022. I installed Server 2019 and it didn't work on that either. I wonder if Siemens claims these systems are compatible without testing them. Everything I've done is according to the original Siemens documentation. I've made all the settings as instructed, but I still can't get the webnavigator client to work. |
7/18/2025 12:33 PM | |
Joined: 8/3/2009 Last visit: 9/15/2025 Posts: 16409 Rating:
|
Hello xoptopus do you have opened already a Service request at Siemens Support? Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on