7/17/2025 1:48 PM | |
Joined: 11/4/2014 Last visit: 7/18/2025 Posts: 2 Rating:
|
Hello, I'm trying to read the output of my digital energy meter with the help of a 1200 CPU in combination with the CM1241 RS232 interface. The meter provides the different data whenever the RTS signal is high and keeps on transmitting the data as long as this is the case. I've set the port characteristic's in the hardware and in the software. I can run the code without any errors, but receive nothing in the buffer. When I look at the help for the RCV_PTP block there is mentioned "The sent data is only available in the receive area when the message has been acknowledged by the relevant communications partner." How do I get this NDR value to become high and receive data in the buffer? Thanks in advance |
Follow us on