7/22/2025 8:17 AM | |
Joined: 8/3/2009 Last visit: 9/9/2025 Posts: 16368 Rating:
|
Hello Ronaldo Junior I think we have to separate this in two steps: 1.) Only the Simatic Net versions that are listed in the compatibility tool are compatible and released with WinCC: https://support.industry.siemens.com/cs/de/en/view/64847781 So check out your specific WinCC Version. 2.) Only since WinCC V7.2 there is a native communicatino driver for a S71500.before this Version a direct communication is not possible. Using OPC UA (WinCC V7.0 Sp3 or newer can act as OPC UA Client) or also the usage of a SIMATIC Net OPC Server (the OPC Server communicates with the S71500 With S7 Protocol) could be an option. But it is not possible to use a direct connection with the S7 Protocol suite channels to a S71500. Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on