7/24/2025 12:29 PM | |
Joined: 1/21/2013 Last visit: 9/11/2025 Posts: 4102 Rating:
|
Hi ahmed_badawi49, Since the "OpenFaceplateInPopup" method within a faceplate type does not bring a parameter to assig interface properties, you can only use inheritance. Any inner type parameters that are also part of the outer type's interface are automatically inherited. For more information, please refer to "Configure faceplate as pop-up". Kind regards |
Follow us on