9/15/2020 3:06 PM | |
Posts: 12 Rating:
|
Hi, mdarende! Did you found an answer? I have the same questions) |
9/27/2023 8:13 AM | |
Joined: 2/6/2015 Last visit: 9/5/2025 Posts: 172 Rating:
|
Thank you so much! |
7/29/2025 1:38 PM | |
Joined: 1/21/2013 Last visit: 8/29/2025 Posts: 4087 Rating:
|
Hi,
To use the GIF file on the panel, place it there. It will not transfer with the project when transferred from TIA Portal. Depending on the target path selected, the web control's URL must be configured. Kind regards |
7/29/2025 2:48 PM | |
Joined: 1/21/2013 Last visit: 8/29/2025 Posts: 4087 Rating:
|
Hi, Unfortunately, the only way to transfer files to the panel is via the File Browser app. The source can be a USB stick, an SD card, or a network share. Kind regards |
This contribution was helpful to
1 thankful Users |
Follow us on