7/31/2025 1:59 PM | |
Joined: 7/24/2025 Last visit: 8/17/2025 Posts: 26 Rating:
|
If I were to use S7 300 PLC would it be ok? |
7/31/2025 2:10 PM | |
Joined: 12/18/2014 Last visit: 9/5/2025 Posts: 35925 Rating:
|
Yes. |
7/31/2025 4:33 PM | |
Joined: 7/24/2025 Last visit: 8/17/2025 Posts: 26 Rating:
|
Thank you for the support! |
This contribution was helpful to
1 thankful Users |
8/2/2025 9:28 AM | |
Joined: 12/27/2006 Last visit: 8/26/2025 Posts: 1200 Rating:
|
You can connect two counters and subtract the value of them sepeately/ Look in the example. The first counter counts 10000, so you can count 10000 x 32000= a lot Notice: The textblock is not perfect. You can make it perfect with several tekstblock, AttachmentHoge telling.zip (37 Downloads) |
Follow us on