7/4/2019 2:49 PM | |
Joined: 3/2/2015 Last visit: 8/25/2025 Posts: 67 Rating:
|
How did you solve this issue. We have same problem. In our case it is WinCC 7.0, and SICAM PAS 7.01. We faced this issue after performing an archive operation in SICAM PAS Configuration viewer (without a configuration license). After archiving when SCC restarted, it showed following message “SICAM PAS Base and SICAM SCC parameter set not compatible Please check the following components with Project ID 1 and SCC Interface address 13” On some troubleshooting, found out that the Global C script "SicamPAS_CompKey.pas" was triggering this message because the compatibility key changed somehow. This script shutdowns run-time on mismatch of compatibility key between PAS and SCC. When I disabled this script, SCC started up, but a couple of tags are now showing wrong values. I couldn't find manuals for SICAM PAS. Could anyone point in the right direction? Regards, Anas ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 07/05/2019 07:58:41New subject after splitting |
|
6/21/2024 11:51 AM | |
Joined: 6/21/2022 Last visit: 4/19/2025 Posts: 3 Rating:
|
Good afternoon, I am experiencing the same issue, did anyone have answers or managed to fix this issue. regard, Likho |
8/30/2025 7:44 AM | |
Joined: 8/30/2025 Last visit: 8/30/2025 Posts: 1 Rating:
|
hello, i have this problem too really appreciate for answers |
Follow us on