9/2/2025 1:45 PM | |
Joined: 8/3/2025 Last visit: 9/7/2025 Posts: 12 Rating:
|
Hello Daniel Chartier Sir, it is my mistake that i have not given complete details for that apology, but Sir now i have made a architecture to understand that what i need, actually no bill is available for available material because it is removed from another process years ago and now i want to upgrade this machine because it has old model s5 so i need complete replacement with s7 400 system now i have clearly define in the picture in attached pdf that i have no IM cards i dont want to use them so is that possible in that way in which i want to communicate as i have shown the profinet link green by not using IM cards what i need only to operate DO and receive DI card status of s7 400 family from rack no.2 and rack no.3 to main cpu rack (master rack) Attachments7 400 architecture.pdf (4 Downloads) |
9/2/2025 7:24 PM | |
Joined: 9/27/2006 Last visit: 9/9/2025 Posts: 12402 Rating:
|
Hello; I think I have deciphered the part number of the CP 443-1 you are using, from one of the earliers posts you published. When you are requesting help on the forum, part numbers are an extremely important information you must provide us with, since the capâcities of the modules evolves over time, and the modules you have might not be able to do the job. Am i correct that it is a 6GK7443-1EX11-0XE0 in your original picture? How about the other CP 443-1 that you would put in the remote racks, are they he same model? If this is the case, please open the file in the attachment below, it shows your data sheet for this model of CP 443-1. Notice that it states nowhere that it can handle Profinet exchanges. It cannot be a Profinet IO controller or a Profinet IO Device, that could allow you to read and write the DI and DO modules in your remote racks. The CP 443-1 you are trying to use was cancelled in 2009, which means that it is not even available as a spare part from Siemens, and that no documentation for it can be located on the siemens site (I had to search the web to locate that datasheet). It was never active when profinet was introduced, and cannot be used as a Proinet interface. Just for your information, the successor product for your CP 443-1, the 6ES7443-1EX31-0XE0, was able to act as a Profinet IO Controller, as per its datasheet. But it still could not be a Profinet IO Device... At this point, I have exhasusted the help I can provide to you on this project. If no one else on the forum steps up to add suggestions, I think that contacting Siemens techs through a Support Request would be your only choice. When you do so, provide them with a complete description of the system you want to build, including all part numbers for the CPU and CPs, if you want realistic answers. Hope this helps, Daniel Chartier Attachment6GK7443-1EX11-0XE0.pdf (2 Downloads) |
Last edited by: dchartier at: 09/02/2025 19:33:57 |
|
This contribution was helpful to
1 thankful Users |
9/5/2025 12:33 PM | |
Joined: 9/27/2006 Last visit: 9/9/2025 Posts: 12402 Rating:
|
Hello; First point, we will never propose "IM cards" for your application. S5 interface modules and cables to connect expansion I/O racks will never work with a S7-400 CPU, S7-400 IMs are not compatible with s5 systems. See this page from the S7-400 Module Data manual for information on S7-400 IMs: https://support.industry.siemens.com/cs/ca/en/view/1117740/94331293835 The only solution we can propose is based on network connections between the S7-400 CPU in your new system and ,Profibus or Profinet (and there are no interface modules for Profinet on S5 systems). But first, to clear up any issues, please provide us with a complete list of all part numbers of the S7-400 system you have on hand, Power supply, CPU, CPs, IO modules... so we can evaluate the capabilities of each, since the S7-400 you want to use appears tpo be outadted, and mioght not be able to accept certain configurations. Until you provide us with such a list, I will nto be able to support you any longer. Another option would be to contact Siemens techs with a Support Request as suggested earlier, add that same list to the request, and explaining very clear;ly waht you want to do with yoru S7 equipoment. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 09/05/2025 12:35:20Last edited by: dchartier at: 09/05/2025 12:43:11 |
|
This contribution was helpful to
1 thankful Users |
9/6/2025 3:56 PM | |
Joined: 9/27/2006 Last visit: 9/9/2025 Posts: 12402 Rating:
|
Hello; Thank you for your equipment list, I will try to see how we vcan help you build a project that will enable you to do what you are planning to do. <I am missing 2 more informations: the part number for the memory card (MC) you will use in the S7-400 CPU (I suggest yo use a RAM card, as described in the foilloweing link) and the version of Step 7 you will work with in this project. https://support.industry.siemens.com/cs/ca/en/view/73159687 Since it does no seem possible to use Profibus or Porifnet to gateher the IO status on your remote racks, I believe we cn use S7 Communications on the Ethernet link between your CP 443-1s, specifically PUT and GET functions. If we are able to program these SFB15 and 14, yoiu would only have to transfer the DI module data to a IN_DB with GET, and the DO data to a OUT_DB to write values through PUT. These appear to be the less complex wayfor your CPU to read and write to every rermop0te IO rack. We can discuss details later. https://support.industry.siemens.com/cs/ca/en/view/23904550/9716620683 Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 09/06/2025 16:12:10 |
|
This contribution was helpful to
1 thankful Users |
Follow us on