8/25/2025 7:23 AM | |
Joined: 11/3/2008 Last visit: 9/5/2025 Posts: 68 Rating:
|
The IP parameters are OK. There may be a lot of different reasons e.g. incompatible OS. For me most likely is the software is too old. Therefore I recommend the upgrade to LOGO!Soft Comfort V8.4.1: https://support.industry.siemens.com/cs/ww/en/view/109975995 Hint: If you are not yet registered, the registration must be carried out beforehand because the software is restricted to export. When registering, the check mark must be set for "Access authorization for downloading export-restricted software", see: https://support.industry.siemens.com/cs/ww/en/view/109744535 |
9/4/2025 5:20 AM | |
Joined: 9/11/2014 Last visit: 9/5/2025 Posts: 867 Rating:
|
Hi, did you check if your LOGO! Soft Comfort Version supports the not working LOGO! type? Best is to do update to the latest LOGO! Soft Comfort update. This version LSC V8.4.1 supports any type of LOGO!. Here the link to the free of charge update to LOGO! Soft Comfort V8.4.1 Note: If you do not use a LOGO! 8.4, then you cannot use the FW update for LOGO!. Hope this helps |
Follow us on