8/20/2025 10:13 AM | |
Joined: 6/4/2018 Last visit: 9/5/2025 Posts: 5 Rating:
|
Good afternoon, I'm trying to install an HSP (HSP_V20_0465_001_S71200G2_Phase2_1.0) on TIA Portal V20, but I'm getting the message “The installation was aborted with errors. The tia portal can now be started again" on the HSP Support Package Installation window. I have already tried different HSP packages on TIA V16 and V20, using both my laptop (TIA V20) and another PC (TIA V20 upd3), and connected as user and admin, but none of these worked. I'm using Windows 11 Pro, version 24H2 (OS Build 26100.4946). I have also attached the latest logfile created in case it helps. This logfile is from the last trial using TIA V20 as administrator. Thanks! ------------------------------------------------------------------------------------------ AttachmentSupportPackageInstallation_202508200937.zip (41 Downloads) |
Last edited by: Moderator_Lan at: 08/20/2025 10:41:51New subject after splitting |
|
8/22/2025 2:24 PM | |
Joined: 11/28/2024 Last visit: 9/6/2025 Posts: 1 Rating:
|
Hi Thanks all, the same worked with me too, run TIA as administrator |
9/4/2025 8:45 AM | |
Joined: 6/18/2020 Last visit: 9/4/2025 Posts: 5 Rating:
|
It is worked for me to after log on with " as an administrator " |
Follow us on