9/4/2025 12:28 PM | |
Joined: 2/10/2015 Last visit: 9/5/2025 Posts: 143 Rating:
|
Hi, here's the manual for RF1040R: https://support.industry.siemens.com/cs/ww/en/view/109978376 First you need to decide on the operating mode of RF1040. See page 33. 1. Unidirectional data receipt without using the programming interface or 2. Read and write user memory
If 1. is sufficient for your use case, the reader will send the data to RF120C as soon as a transponder is presented. The presence Bit and LED will indicate new data, that can be obtained using the Read command. In this case you'll need to load a configuration into the RF1040R using the config editor. |
Last edited by: AutoGen_242158 at: 09/04/2025 12:29:28Last edited by: AutoGen_242158 at: 09/04/2025 12:30:03Last edited by: AutoGen_242158 at: 09/05/2025 15:10:36 |
|
9/5/2025 11:50 AM | |
Joined: 8/13/2024 Last visit: 9/5/2025 Posts: 4 Rating:
|
This is my first project with such a hardware configuration. I have been trying to do something for 2 days but there are no results. I installed all the programs, tried to configure RF1040r, reread many pdf files but again the result did not go further than what I came here with. |
9/5/2025 1:42 PM | |
Joined: 2/10/2015 Last visit: 9/5/2025 Posts: 143 Rating:
|
Is 1. (Unidirectional data receipt without using the programming interface) sufficient for your use case? Is the UID or some Bytes of Data all you need? Maybe you can share your config? |
Last edited by: AutoGen_242158 at: 09/05/2025 13:45:36Last edited by: AutoGen_242158 at: 09/05/2025 15:09:55Last edited by: AutoGen_242158 at: 09/05/2025 15:10:13 |
|
Follow us on