9/10/2025 9:48 AM | |
Joined: 5/24/2016 Last visit: 9/11/2025 Posts: 412 Rating:
|
Hello. Could you please provide us with the motor order number on this axis. Best Regards Riddersholm |
9/11/2025 5:31 PM | |
Joined: 9/9/2025 Last visit: 9/13/2025 Posts: 4 Rating:
|
https://photos.google.com/photo/AF1QipMLu0GumxPQ_ypOpmc-b0ODkLbZpwXHnFg4nhe_ https://photos.google.com/photo/AF1QipPIJLYQHD54CmSqgx2_AEdcJ8SKE-IIviUwmSUI I couldn't insert the image into the pager. I'm sending the links. When setting it up, I changed it to "0". Then I restored it to the previous value. Everything worked fine after the reconfiguration until the power was disconnected from the machine. This happened a few days later. And I'm also sending the instructions I used to do this. |
9/11/2025 8:56 PM | |
Joined: 10/17/2007 Last visit: 9/12/2025 Posts: 4449 Rating:
|
I click your links return to me 404 error, can you check these MD 30240[0]=? MD30240[1]=?
|
If you like my comments please |
|
Follow us on