9/3/2025 6:23 AM | |
Joined: 8/3/2009 Last visit: 9/15/2025 Posts: 16409 Rating:
|
Hello Furkanayeng One general way would be to use the Option Audit: https://docs.tia.siemens.cloud/r/en-us/v20/wincc-audit-rt-unified But this Option is not available for Unfied Basic Panels (only for PC RT and Unified Comfort Panels) so you habe to use the alarm logging system. There are possibilities to generate operator messages by script. For example if the @UserName systemtag changes (login and logout) or if an operator input or operation takes place. Bye Murof |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
1 thankful Users |
Follow us on