9/5/2025 6:44 AM | |
Joined: 9/30/2021 Last visit: 9/10/2025 Posts: 13 Rating:
|
Hello, I'll get into this conversation because I'm having the same problem now and I can't manage to resolve it. I've been trying to run a simulation of a WinCC Unified comfort panel for the last week and I can't manage to do it. The first problem I got told me that the runtime simulation version didn't match with the TIA Portal version (even though both of them had the UPD2 installed) and it dind't change anything even after reinstalling both TIA Portal and WinCC Unified Runtime. So I tried to use a totally new virtual machine to start from zero and after installing TIA Portal V20 and WinCC Unified Runtime V20 without any updates it worked just fine. The same problem that “ghhgkjlkékjlghj” issued appeared after installing the UPD2 for both software. Now I tried:
I'm looking forward for a response. ------------------------------------------------------------------------------------------ |
Last edited by: Wit_Moderator at: 09/05/2025 10:24:02New subject after splitting |
|
9/9/2025 8:42 AM | |
Joined: 8/3/2009 Last visit: 9/16/2025 Posts: 16411 Rating:
|
Hello Mirko_C Check again in yuor installed SW for the latest versions you should have at the moment: (you can see it in Installed SW in TIA Portal and then -> detailed information about instanned software-> Products ) Which Error message do you get if you want to simulate? (if you select device Version V20.0.0.0 and V20.0.0.2)? I can say on my system this works without problems. Check also if you have set up your Runtime properly: https://support.industry.siemens.com/cs/de/en/view/109806850 Bye Murof |
Last edited by: Murof at: 09/09/2025 08:43:11If this Information really helps, you could use the Rate function |
|
Follow us on