(0)| 12/2/2025 7:14 AM | |
|
Joined: 7/31/2020 Last visit: 12/10/2025 Posts: 360 Rating:
|
Hello, Are you familiar with the following articles on communication between CPU and HMI? Connecting older HMI to S7-1500/1200 with newer firmware No connection to PLC after WinCC Panel Images V17 Update 6 Fix Certificate Error between HMI Unified Panel and SIMATIC S7-1500/S7-1200 or Software Controller Best regards |
| 12/2/2025 7:55 AM | |
|
Joined: 1/21/2013 Last visit: 12/10/2025 Posts: 4323 Rating:
|
Hi dsi-eng, As far as I know, the NetExtender VPN server is integrated with SonicWall firewalls. Therefore, I would assume that a firewall rule is blocking the traffic. Perhaps a firewall administrator could check if the ports used by WinCC Panels are available. However, going online with a panel is a rather useless task since you will not be able to obtain usable information. Are you having trouble downloading to the panel or connecting using Sm@rt Client? Kind regards |
| 12/3/2025 2:26 PM | |
|
Joined: 8/18/2025 Last visit: 12/10/2025 Posts: 11 Rating:
|
Hi Tarwar, Yes, I am familiar with this. The PLC and HMI communication is fine. |
| 12/3/2025 2:30 PM | |
|
Joined: 8/18/2025 Last visit: 12/10/2025 Posts: 11 Rating:
|
Attached image show the fail connection via TIA PORTAL |
Last edited by: dsi-eng at: 12/03/2025 14:31:53 |
|
Follow us on