(1)| 5/23/2022 3:18 PM | |
|
Posts: 5 Rating:
|
Hello everyone, I want to transfer Data logging, Audit logging, alarm logging CSV file from HMI local storage to Clients centralized PC. I have TP700 comfort panel. All the setting which i did , I attached in Attachment. after that setting HMI not able to find the PC folder path to save file. what setting i am missing please suggest me. following document i reffered: 1. 92346478_TCP_IP_Networks_Panel_DOC_v2.0.en 2.92346478_WinCC_TIA_Archiving_ServerNAS_DOC_v2.0_en Attachmentsettings.pdf (1172 Downloads) |
| 7/4/2024 7:41 AM | |
|
Joined: 6/26/2024 Last visit: 1/9/2026 Posts: 1 Rating:
|
Is you problem solved????if yes can you tell me how you are solved it pls |
| 1/4/2026 8:49 AM | |
|
Joined: 12/6/2024 Last visit: 1/4/2026 Posts: 1 Rating:
|
I AM ALSO FACING THIS SAME ISSUE |
| 1/6/2026 8:40 AM | |
|
Joined: 7/5/2013 Last visit: 1/12/2026 Posts: 3274 Rating:
|
Hi all, I would avoid SMB v1.0 and use Option+ instead for transfering files from panel to a shared directory: Integrating HMI Operator Panels in TCP/IP Networks and access to a NAS or to a shared Windows folder and data exchange via "SIMATIC Option+ Manager". Regards, Frink |
|
Pi is exactly three! |
|
Follow us on