(0)| 1/22/2026 1:47 PM | |
|
Joined: 1/21/2026 Last visit: 1/22/2026 Posts: 2 Rating:
|
Dear Technology Team, I would like to express my serious concern regarding the practical usability of the PDC series when driving BLDC (EC) motors with Hall sensor feedback only. In industrial practice, the vast majority of BLDC motors are equipped with Hall sensors and are operated without encoders. Therefore, it is highly unexpected that a BLDC motor drive would not function correctly in such a configuration. I must note that this situation may fall under the scope of misleading information as defined by applicable consumer protection regulations. ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 01/22/2026 16:06:08New subject after splitting |
|
| 1/22/2026 4:06 PM | |
|
Joined: 7/30/2024 Last visit: 1/23/2026 Posts: 1207 Rating:
|
Topic closed, because the issue was raised twice. The active topic can be found here: PDC-100 serious technical issue Kind regards, Moderator_Lan |
Follow us on