7/10/2009 9:57 AM | |
Joined: 9/27/2007 Last visit: 12/18/2020 Posts: 993 Rating:
|
Hi The property "ToolbarButtonClick"is available in Controls(p. E. AlarmControl). Here an describtion: http://support.automation.siemens.com/WW/view/en/11769423 Which toolbar you will access? Do you want to get an event or do you want to set an even like in the posted entrie? regards cumulus |
Learn more about visualization - visit the HMI courses of Siemens AG! |
|
7/14/2009 9:16 PM | |
Posts: 55 Rating:
|
Hello, cumulus I need to access Status bar, object ID 2 - CurrentListMessagesCount. Would you provide a example in C script? Thank you awu10 |
7/15/2009 2:50 PM | |
Joined: 9/27/2007 Last visit: 12/18/2020 Posts: 993 Rating:
|
Hi here is an Entry, which use the same function: http://support.automation.siemens.com/WW/view/en/7797013 regards cumulus |
Learn more about visualization - visit the HMI courses of Siemens AG! |
|
7/16/2009 10:41 AM | |
Joined: 9/27/2007 Last visit: 12/18/2020 Posts: 993 Rating:
|
Hi
|
Learn more about visualization - visit the HMI courses of Siemens AG! |
|
This contribution was helpful to
1 thankful Users |
7/27/2009 11:20 AM | |
Joined: 9/27/2007 Last visit: 12/18/2020 Posts: 993 Rating:
|
Hi You changed the GMsgFunction.fct (WinCC standard function) or is GMsgFunc.fct your own function (project function)? You do not use the Classic control. You problem will be the trigger of the skript or the rigth ElementID. For testing i would advice you to run th skript by buttonclick, so you can look if you use the rigth ID. For normal use you should use a event of the AlarmControl to trigger the skript. I am not sure which is the rigth one, you shoud test it to. regards cumulus |
Learn more about visualization - visit the HMI courses of Siemens AG! |
|
Follow us on