(2)| 7/24/2009 9:02 AM | |
|
Posts: 37 Rating:
|
Hi Iam using DP-DP Coupler for communication between S7-400 & S7-300 CPU. CPU 315-2DP. MLFB - 315-2AG10-0AB0. CPU 400-- 6ES7-414-3XM05-0AB0. Can MPI port of 300 CPU be connected to DP-Dp Coupler? . If it would have to be connected on DP port then how to do programming ofCPU 300?.i want to do programming through Ethernet port of S7-400 CPU.pls see the attachedautomation configuration AttachmentDP DP Coupler.zip (356 Downloads) |
| 7/27/2009 9:07 AM | |||
|
Joined: 9/27/2006 Last visit: 1/16/2026 Posts: 12481 Rating:
|
Hello himanshu; Have a look at the following FAQ, it discusses MPI connections and data exchanges. It also provides links to sample configurations so you can develop your application as per your requirements. http://support.automation.siemens.com/WW/view/en/21537047 Hope this helps, Daniel Chartier Edit, after examining your Excel file: One more point: You cannot use OLMs with MPI in order to extend the length of the network. http://support.automation.siemens.com/WW/view/en/8574670 You can use a repeater (and copper cable)for that purpose, but only up to 50 m (on standard S7-300 MPI ports): http://support.automation.siemens.com/WW/view/en/37627 Also: for your “ET S7-300” units, which I presume are ET 200M interface modules with S7-300 SMs, there is an IM 153-2 FO module that would allow you to connect your Profibus-DP FO directly, without an additional OLM:
Regards, DC |
||
Last edited by: dchartier at: 7/27/2009 9:35 AMLast edited by: dchartier at: 7/27/2009 9:34 AM |
|||
| 8/5/2009 11:36 AM | |
|
Posts: 37 Rating:
|
I could possibly transfer data with MPI Port between 400 CPU & 300 CPU with help of SFC 67 & SFC 68. FO Connection is there between MPI link of both CPU. But the data transfer is somewhat slow. how to improve response .Please help me what input to be given in REQ & CONT inp of SFC 67 & SFC 68, whether fix or variable. In my project i had given permanent HIGH input to REQ and permanently LOW input to CONT input. Please see attachment.
AttachmentSFC 67&68.pdf (361 Downloads) |
Follow us on