9/8/2009 8:35 AM | |
Joined: 4/5/2006 Last visit: 7/30/2025 Posts: 917 Rating:
|
Hi Machonish , the disable key function if for the project and for ALL users (not possible define different function for different users) What you can do is define buttons with script to execute external program like "Task Manager" or "Windows Explorer" and more.....Set privilege level on this buttons Hope can help Regards |
This contribution was helpful to
1 thankful Users |
9/8/2009 11:46 AM | |
Posts: 76 Rating:
|
when you press on button "User Administrator" then control panel is visible and u get access to OS Windows |
Follow us on