(0)| 9/9/2009 10:03 AM | |
|
Joined: 4/5/2006 Last visit: 10/3/2025 Posts: 917 Rating:
|
Hi Testermax , what you did is the right PCS7 filosophy. the others way to do that are: 1) create an user DataBlock, right click to select "Special Object properies" --> "Operator Control and Monitoring" and check bock. Create nr. 2 binaty tags (for example "set" & "reset"), for each oneright click and select "Object properies" to set attribute "S7_m_c" "true" (take care about uppercase sintax). Save and compile, then you have tags "set" & "reset" in WinCC database. 2) it possibile create a simple in "SCL" or "STL" language to create a simple block with same "S7_m_c" attribute to send tags in WinCC database. YOu can find basic information in PCS7 help in manual "S7-SCL - Working with S7-SCL" P.S.: what Yersaid is also right. Better use an edge to make Set/Reset FF Hope can help, Regards |
Last edited by: CBo at: 9/9/2009 10:06 AM |
|
| 9/9/2009 2:31 PM | |
|
Posts: 159 Rating:
|
Hi and thanx for quick reply!! I tried #1 at first but for some reason it didnt work! Tried again and then the db showed up in winCC! |
Follow us on