9/24/2009 12:50 PM | |
Posts: 15 Rating:
|
no, it's the Wincc V6.2 sp2. |
9/24/2009 9:24 PM | |
Posts: 2661 Rating:
|
Hi fredaster, You have not mentioned if you were able to download to the OS successfully. It is vital that after you download you should wait for "Download Successful" pop-up window (which sometimes takes several minutes), click on OK and only then attempt to open the project on the OS. Also see the following FAQ's: Which settings should you check if OS downloading fails with PCS 7 or the OS project cannot be activated? How can you clear the error message "Download (310:88)"? Regards |
Follow us on