(0)| 10/1/2009 1:53 PM | |
|
Posts: 535 Rating:
|
Dear Oscar_83PL, another possibility is to use the FBs as multi-instances. Therefor you have to call the 'heater-FB' from another FB (both FBs must possess multiple instance capability). In the calling FB you now can add the heater-FB in the STAT-section of the block-interface and call this instance in your code. (Have a look at this article). Please observe, that this increases the size of the calling FB-interface and the instance-DBs (maximum size of the DB depends on the CPU, but is max. 64 kB). Best regards, yy1 |
This contribution was helpful to
|
|
Follow us on