(0)| 9/29/2009 9:16 AM | |
|
Joined: 4/5/2006 Last visit: 10/3/2025 Posts: 917 Rating:
|
Hi Delphoe, It's possible Backup and Restore Batch database byBatchControlCenter menu: it's possible bachup/restoreall database. It's possible to use Import/Export function also (available from SImatch Batch v6.0 - if i remeber well): in this case Import/Export doesn't dsavebatch (doesn't matter if progress orcompeted).
I'm talking about internal function, if you want to use a different way to manage SQL2005 database i think you have to ask directly to you customer support Im sure if you explain them your application you are going to develop, they can support you stongher. SIMATIC Batch is not so easy to understand very well without tutor or quick course if you already expert in PCS7 Hope can help, Regards |
| 10/2/2009 9:10 AM | |
|
Joined: 4/5/2006 Last visit: 10/3/2025 Posts: 917 Rating:
|
Hi Delphoe,
That is not BF database but WinCC Historical data (coming from Alarm Logging and Tag Logging configuration). Batch closed has to be stored manually in forlder you select in BF option menu (archive folrder). With SBR it possible view all Batches still in Batch database and Batch exported. When Batch is in complete status, operator has to close it (during this time BF read all historical data with Batch related and store them in proper batch report), then archive. After that, openening the srored file with SBR you'll be able to see all event (opeartor message, alarm, trend when configured). Hope can help Regards |
Follow us on