10/6/2009 1:43 AM | |
Posts: 2661 Rating:
|
Hi Donehill, Can you explain what certain operators willaccomplish by accessing the desktop? If it is matter of storing files you can program buttons in WinCC (with proper user rights) to enable read/write of files. See following thread: Editing/Saving example.txt file from WINCC |
10/6/2009 8:24 AM | |
Joined: 4/5/2006 Last visit: 7/30/2025 Posts: 917 Rating:
|
Hi Donehill , in addition what Phantom75said, you can program button with "high users right" just to call application like Explorer, Task Manager and other just using "Progamexecute" function. Only user with "high user right" can access to external application and Desktop in this way (without disable WinCC system hot key) Regards |
Follow us on