10/15/2009 11:46 AM | |
Posts: 27 Rating:
|
Dear All, Ihave queries in Wincc & Hot redundant PLC connectivity. There are 3 redundant PLC stations[414H CPUs & 443-1 CPs (Ethernet)] andi need to connect theseinto one Wincc (V6.2). Do we need to configure in netpro (Simatic manager) or we can assign the individual connections in Wincc. I haveattached the system architecture for your perusal.Our requirement is if any of the CP or CPU fails the Wincc must be able to switch connectiontothe alternate for continuous monitoring.Please advice. Best regards, Dinakaran.
AttachmentS7 414H + WINCC.pdf (98 Downloads) |
Follow us on