(1)| 10/27/2009 3:41 PM | |
|
Posts: 9 Rating:
|
Hello I want to install High Speed analog input card (134-4GB62-0AB0) into one ofmy ET200 node but when I make "Save and Compile" I get consistency error: "Caution: in station 90 WE_LSUW_75_r8 there are additional nodes that also have to be reloaded". What does it mean that additional nodes must be reloaded? If I install predecessor module 134-4GB61-0AB0 everything is ok. Could anybody look at attachments where I put error message text and exported hardware configuration? Thank you in advance. macio Attachmenthardware configuration.zip (380 Downloads) |
| 10/28/2009 1:44 AM | |
|
Joined: 10/7/2005 Last visit: 1/19/2026 Posts: 3054 Rating:
|
Hello macio you do really only have one "problem" in your HWconfig which istheHWconfig error message: "The submodule "2AI I 4WIRE HS" cannot be configured in this slave (slot 42 in slave with PROFIBUS address 61, DP master system 1)" is caused by trying to use a 6ES7134-4GB62-0AB0 AI card in a 6ES7151-1AA03-0AB0 IM151-1. This IM151-1 does howeverNOT allow usage of this AI card (the predecessor AI card 6ES7134-4GB61-0AB0 can be used in it, note too that the 4GB62AI card does NOT exist in the IM151-1AA03 folder either, so I presume you must have dragged in it from a different IM151 model folder). Note further that - for reasons that only can Siemens explain - the 4GB62 AI has a "limited compatibility" to the4GB61. THIS LINK has more details on this subject. The NetPro warnings "Caution: in station xyzare additional nodes that also have to be reloaded"that you also get arejust"friendly reminders". Theirpurpose is to let you know that in case you do change bus parameters you should (must) download to all stations on the network to ensure that they all operate with the sameparameters. I hope this helps |
|
Cheers |
|
Follow us on