(0)| 11/8/2009 9:37 PM | |
|
Posts: 11 Rating:
|
Hi sir I have two cpu315-2DP in software redundant mode(6ES7315-2AG10-0AB0)&two IM153-2(153-2BA00-0XB0). My problem: In my project I have 16 valve that must be opened or closed. I have one FB special for valves & each valve has special DB for itself. Sometimes when a command must changed the bit of DB,but it dosen't happen. In online mode you can see that for example db10.dbx0.0 in program changed to 1,but after opening the DB value of bit isn't changed. for solving that for example valve opened,i must open DB & go to online & download to plc. this solution is useful for one time & for another action for valve imust do again. I must tell this situation sometimes happen. Please solve my problem. Thanks H.pelavar Attachments7_LD.zip (274 Downloads) |
Last edited by: HAMPEL at: 11/9/2009 5:46 AMi attached my s7 program. |
|
Follow us on