(3)| 11/11/2009 12:15 PM | |
|
Joined: 8/25/2005 Last visit: 1/14/2026 Posts: 1162 Rating:
|
Hello motogateDP, hope that I could answer a part of your questions About the GAP list: An example: Your master got adress 2. The next active Station got PROFIBUS-Address 10. So your master will check the adresses 3 up to 9 wether there are new activ stations. The Station with the Address 10 will check addresses 11 and so on. About Starting communication: First of all the master listen to the bus to built his LAS (and his GAP list). Onlylistening. When this list is build he will be able to answer to a telegram where the active station with the lower address is asking about new stations. After this answer the station with the lower address will send him the "token". Now our new master will be able to start his communication with his slaves. About cycle time and so on: have a look at the typical cycle time at the bus and your CPU. Normally bus is faster than the CPU. So you allways will get very actuall data. The master will provide allways the most actuall data to the CPU which he got. Within this manual you will find a documention how it work. SIMATIC NET PROFIBUS Network Manual System Manual Maybe it is a little bit difficult to follow up my description. Sorry, I'm not native english speaker Best regards Sabine |
| 11/12/2009 8:39 AM | |
|
Joined: 10/7/2005 Last visit: 1/15/2026 Posts: 3054 Rating:
|
Hello motogateDP have a look at this (free) Web based animated training course, I have a feeling you will like it (it is well done and detailed): Profibus International Web based training I hope this helps |
|
Cheers |
|
| 11/12/2009 12:27 PM | |
|
Posts: 26 Rating:
|
Thanks a lot guys, now I got it clear. The profibus web training looks very nice. |
This contribution was helpful to
|
|
Follow us on