11/9/2009 10:18 AM | |
Joined: 7/2/2008 Last visit: 8/7/2025 Posts: 928 Rating:
|
Hello Maha, To the best of my knowledge, you can't download individual blocks to flash memory card. You can't even download to flash card unless CPU is in STOP mode. When you edit some blocks and download them, you just download them to worm memory of CPU not to flash card. Please check the attached PDF. Best regards. H-H AttachmentFlash or RAM.pdf (1916 Downloads) |
This contribution was helpful to
2 thankful Users |
11/9/2009 4:23 PM | |
Posts: 947 Rating:
|
In the flash-memory S7-400 can not load the blocks separately. In the flash-memory can only be recorded all the blocks. How make -see in Pdf. flash-memory will be completely rewritten
Attachmentflash.pdf (1314 Downloads) |
This contribution was helpful to
1 thankful Users |
Follow us on