8/7/2006 10:04 AM | |
Joined: 9/27/2005 Last visit: 11/27/2007 Posts: 1398 Rating:
|
WinCC has two types of clients - Client With Project and Clients Without Project. I believe that you should only use a Client With Project with a dial-up connection. You can find more information about the two types of clients in the WinCC manual. However ... have you considered using a web client ? WinCC offers two options for web clients : 1) WebNavigator - a full control WinCC client that runs within Internet Explorer 2) DataMonitor - a read-only (view) WinCC client that runs within Internet Explorer These clients require a lot less bandwidth compared to a standard client and are ideal for dial-up connections. You can find more information about these options on this forum, in theProductSupportarea of this website and at http://www.siemens.com/wincc/options |
Follow us on