(0)| 12/30/2009 9:05 AM | |
|
Joined: 4/24/2006 Last visit: 1/20/2026 Posts: 9106 Rating:
|
Dear SNB, No, you can not use WinCC flexible 2008 to develop for WinCC flexible 2007 RT. You can use the option (Save as version), but it will only be possible to go back one version. (And sometimes a Service Pack can be a version) But you will need WinCC flexible 2007 Advanced to compile the project to a Runtime application. Perhaps you have WinCC flexible 2007 Advanced, you can install it on another PC or in Virtual machine. You can use the Floating License of WinCC flexible 2008 Advanced to work with WinCC flexibel 2007 Advanced See also these links: What are the solutions offered for working with different versions of WinCC flexible? how can you save WinCC flexible project/libraries as projects/libraries in the format of an earlier version of WinCC flexible? Best regards, Wizard |
Follow us on