(0)| 2/9/2010 4:08 AM | |
|
Joined: 5/28/2008 Last visit: 1/14/2026 Posts: 4522 Rating:
|
Hello Viks_fj, Welcome to Siemens world, I hope the following links will help you: SIMATIC PLC S7-300, CPU Specifications CPU 312 IFM to CPU 318-2 DP S7-300 Automation System, Hardware and Installation: CPU 312IFM - 318-2 DP Also please note that the mentioned CPU is phased out Product Phase-Out for SIMATIC S7-300 CPU 312IFM and 314IFM Hope this helps. |
|
Ayman Elotaify |
|
| 2/9/2010 10:34 AM | |
|
Joined: 7/2/2008 Last visit: 12/21/2025 Posts: 929 Rating:
|
Hello Viks_fj,
You have the manuals now thanks to Mr. Ayman's contribution. I recommend to take a look at Guided Tourwhere you can learn how to search here (Look at guided tour Search).
The CPU itself doesn't have an Ethernet port however it can beconnected to an Ethernet network through a CP (Communication Processor). The S7-300 platform has 3 types of Ethernet CPs. You can find differences between them in the industrial communication catalog. If you are going for just monitoring and programming over TCP/IP network then I recommend the entry level CP343-1 Lean. Best regards. H-H |
Follow us on