(0)| 1/30/2010 7:04 AM | |
|
Posts: 22 Rating:
|
Dear Sir, Greetings of the day. Sometime back we used Telecontrol Module VICOS RTU TIM 3V BN (MLFB No. 6NH7808-3AA00) to comply the IEC protocol IEC60870-5-101/104 with physical connectivity RS232. We eastablished the communication with SCADA over this protocol successfully. Please find attached Signal list with signal Type & Type ID. Now there are some more MDBs are going to add with same specification & signal list. But Siemens has made TIM 3V BN (MLFB No. 6NH7808-3AA00) phase out. Siemens proposed the alternative TIM 3V IE (MLFB No. 6NH7808-3BA00). Can you please clarify me following queries. 1. Will the new module work in the same way as of Old? 2. We are using ParaM softwere to configure the TIM. The same software can be be used to configure the new module? 3. Is there any additional parts needs to procure with this module? 4. Is there any change in software programming? Thanks & Regards Praveen Patil, Manager - Projects GULF COAST, ELECTROMECHANICAL INSTALLATION WORKS LLC, SIEMENS SYSTEM INTEGRATORS 103,Abdul Al Fahed Building, Al Nahda Street, Quasis, Dubai - UAE. Tel/Fax:+971-4-2612133 Mobile:+971-50-4947876 Email:- pravin.patil@foxindia.net Web: www.foxindia.net AttachmentMDB Signal list__LV SCADA System Rev 1.0.pdf (288 Downloads) |
Follow us on