(0)| 2/16/2010 1:36 AM | |
|
Joined: 10/7/2005 Last visit: 1/20/2026 Posts: 3054 Rating:
|
you are correctdear lazywhiteboyand can NOT use the CP5431 as aDP Slave.
Don't worry about this terminal, it is optional to use them. For completeness, the current part numbers for the various versions of theseterminals are: 6GK1 500-0DA00 6GK1 500-0AB00 6GK1 500-0AA00
Assuming your DCS is a Profibus Master, you canexchange up to 244 Bytes of data both ways between it and the S5 by addingan IM308C to your S5 and configuring it as a DP Slave. Below are some links which will give you more info on this and should help in getting you started: ET 200 Distributed I/O System with IM 308-C Manual How do you operate an S5 (with IM 308-C) as a DP slave on the PROFIBUS DP when the DP master is an S7-300/400?(Note: Your DCS will take the role of the DP Master). I hope this helps |
|
Cheers |
|
Follow us on