(0)| 4/1/2010 2:11 PM | |
|
Joined: 10/7/2005 Last visit: 1/21/2026 Posts: 3054 Rating:
|
Hello lambertws you are correct, the CPU928(B) does NOT support the IAE command. I can't unfortunately tell youhow it behaves if it tries to execute a Block that has the IAE command init (I never tried this for somewhat obvious reasons). I would expect that it will cause a so called Operation code error and call OB29, butwith IAE being a system command it may perhaps also simplyignore it (e.g. treat it as a NULL operation). Perhaps other forum users have tried this and know for sure and cantell you. Just in caseyour program is actually from a 948 CPU, the IAEcommand will disable addressing errors (and OB25 calls)until such time that an RAE command is executed. I hope this helps |
|
Cheers |
|
| 4/6/2010 11:54 AM | |
|
Posts: 58 Rating:
|
Thanks for the reply Fritz. I will make the conversion in case the IAEs work and make them as comments for a while until I can do some trial. |
Follow us on