(0)| 4/25/2010 5:48 PM | |
|
Joined: 4/24/2010 Last visit: 12/23/2025 Posts: 16 Rating:
|
I arleady connect PLC 224 to MM410(ON OFF1 OFF2 Change dir ok.But when i use USS_WPM_W to change value in P2000 i MM410 it does not effect P0003=3 P1000 Index 0=5 P2009 Index 0=0 Attachmentuss.zip (187 Downloads) |
| 4/26/2010 8:06 AM | |
|
Joined: 4/24/2009 Last visit: 8/20/2024 Posts: 2682 Rating:
|
Thread closed, because question is already published in the following thread Connect PLC 224 to MM410 Use USS Protocol???. Best regards O_Moderator |
Follow us on