(0)| 5/24/2010 2:11 AM | |
|
Joined: 10/7/2005 Last visit: 1/20/2026 Posts: 3054 Rating:
|
Hello ghost_dc could it be that the Inputs you are trying to read from flex are outside the Process Image of the CPU but configured as if they were inside it? If so please add a "P" in front theflex input address? |
Last edited by: fritz at: 5/24/2010 2:34 AMCheers |
|
| 6/2/2010 2:09 PM | |
|
Posts: 1 Rating:
|
Sir, Please ensure that the tag changes its value in the PLC(Variable Table). If so, then delete the tag in WinCC Flex and create it again with the same address. |
Follow us on