(1)| 6/2/2010 5:08 AM | |||
|
Joined: 9/27/2006 Last visit: 1/15/2026 Posts: 12481 Rating:
|
Hello anshul: First the part number you mwention is not quite right. Look at the following:
The Masterdrive VC Compendium (the VC bible): contains all parameter and communication information http://support.automation.siemens.com/WW/view/en/13472409 The required Profibus interface: CBP2(part no, 6SX7010-0FF05) The GSD file for CBP2 isinserted in Step 7 HWConfig editor only after installation of the Drive-ES Basic package: http://support.automation.siemens.com/WW/view/en/6945208 http://support.automation.siemens.com/WW/view/en/23516036 Hope this helps, Daniel Chartier |
||
| 6/4/2010 10:50 AM | |
|
Posts: 151 Rating:
|
For all Masterdrives 6SE70, all DC-Master 6RA70 and some other ones, too, there is only one GSD file, because for all Masterdrives... there is only one CommBoardProfibus CBPx (old CBP 6SE7090-0XX84-0FF0, new CBP2 6SE7090-0XX84-0FF5), or 6SX7010-0FF00 / 6SX7010-0FF05. AttachmentMD DC DES_Hardware.zip (383 Downloads) |
This contribution was helpful to
|
|
| 6/7/2010 9:14 AM | |
|
Joined: 4/24/2009 Last visit: 8/20/2024 Posts: 2682 Rating:
|
Thread closed, because question is already published in the following thread master drive programming. Best regards O_Moderator |
Follow us on