(0)| 6/10/2010 3:09 PM | |
|
Joined: 4/5/2006 Last visit: 10/3/2025 Posts: 917 Rating:
|
Hi yac, if you are using PCS7 v6.1 you need to use same CD/DVD to install WebNavigator also. PCS7 and WinCC native works a lil different. i didn't understand where you installed WinCC 6.0 SP4: - if you installed over PCS7 station you need to remove all PCS7 application and reinstall (if doesn't works you need to reinstall the station anew) - if you installed over WebNavigator station, unistall and reinstall from PCS7 CD/DVD. here the compatibility list With what are SIMATIC PCS 7 V7.x, V 6.x, V5.x and V4.x compatible? reagrds |
Follow us on