(1)| 6/21/2010 3:24 PM | |
|
Joined: 7/8/2009 Last visit: 6/7/2025 Posts: 1977 Rating:
|
Hey what are you using for AOP communication? Is it connected with door mounting kit?? If yes, then that might not work as door mounting kit will use RS485 protocol from com link of drive and Profibus Module will also communicate on COM Link. Priority is given to CB so your AOP will not communicate on RS485. Atleast thats what Manual says..... Please refer following thread and attached Manual file... https://www.automation.siemens.com/tf/WW/en/Posts/20481 This is only case if you connect one AOP to all 6 drive using RS 485. If you simply using RS 232 on BOP link, check as Grame said Regards, Devesh Vithani Attachment440_OPI_24294529_en_1006.pdf (329 Downloads) |
Last edited by: Vithani at: 6/21/2010 3:26 PMI dont Like people driving Fast, thats the reason I overtake them ;) |
|
Follow us on