(0)| 6/21/2010 5:43 PM | |
|
Joined: 9/27/2006 Last visit: 1/16/2026 Posts: 12481 Rating:
|
Hello Solution Riders; You are asking questions that go deep inside the PCS 7 configuration, and that could require a lot of research. For starters, you could look at the following FAQ, very detailed: http://support.automation.siemens.com/WW/view/en/19353091How do you create a SIMATIC PCS 7 V6.0 SP3 project with S7-400 station, pair of redundant servers and client? You will alsofind there a link to the Applications section of Siemens Support that will give you pointers on how these configurations can be used for a PCS 7 v. 7 configuration. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 6/21/2010 8:12 PM |
|
This contribution was helpful to
|
|
| 6/21/2010 7:51 PM | |
|
Posts: 385 Rating:
|
Hi Solution riders The manul is too helpful.SIMATIC Process Control System PCS 7 Compendium Part A - Configuration Guidelines Regards |
| 6/23/2010 6:21 AM | |
|
Posts: 1525 Rating:
|
Hi Solution Riders, Here is the link for the Minimal Configuration PCS 7 V7.1,Which will help you for the Configuration. |
| 6/23/2010 10:21 AM | |
|
Posts: 215 Rating:
|
Hi, Treat ES/OS as stand alone in your project & configure it as normal PC station. Dont mix ES/OS with server/Client. |
| 6/24/2010 2:44 PM | |
|
Posts: 112 Rating:
|
dear friends, Can i have the pdf document for assigning of server data package....?. |
Follow us on