(0)| 7/12/2010 9:21 PM | |
|
Joined: 9/27/2006 Last visit: 1/14/2026 Posts: 12481 Rating:
|
Congratulations, and welcome to the forum. .
Yes there are... .
Since your description of the problems is very sketchy, the best thing I can suggest at this time is to read the chapter on Diagnostics from the following manual (Programming with Step 7 v. 5.4): http://support.automation.siemens.com/WW/view/en/18652056 It is quite complete, and will give you many hints on troubleshooting the PLC. Of course, the rest of the manual could be of help too, it covers hardware configuration and programming issues that could help you out. Once you have an idea on how to check the hardware and software issues on your CPU, come back to the forum with more details on your problem. Hope this helps, Daniel Chartier |
Follow us on